Other Parts Discussed in Thread: TPS7A30
Hi team,
Do we have any negative LDO which can support -1V 100mA output?
TPS723 seems to be the closest one.
Best,
Zeming
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Zeming,
The TPS723 would work, but I would recommend using the TPS7A30 for some improved performance.
| TPS723 | TPS7A30 | |
| AEC Q100 | NO | NO |
| Output Options | Adjustable Output, Fixed Output, Negative Output | Adjustable Output, Negative Output |
| Iout (Max) (A) | 0.2 | 0.2 |
| Vin (Max) (V) | -2.7 | -3 |
| Vin (Min) (V) | -10 | -36 |
| Vout (Max) (V) | -1.2 | -1.2 |
| Vout (Min) (V) | -9.75 | -33 |
| Fixed Output Options (V) | -2.5 | - |
| Enable | YES | YES |
| Power Good | NO | NO |
| Output Capacitor Type | Ceramic | Ceramic |
| PSRR @ 100KHz (dB) | 48 | 55 |
| Noise (uVrms) | 60 | 15 |
| Accuracy (%) | 2 | 2.5 |
| Vdo (Typ) (mV) | 280 | 216 |
| Iq (Typ) (mA) | 0.13 | 0.05 |
| Thermal Resistance θJA (°C/W) | 195 | 48 |
| Min Package Area (mm2) | 4 | 9 |
| Package Type | SOT-23-THIN, SOT-23, WSON | HVSSOP, SON |
Thanks,
McKyla