Other Parts Discussed in Thread: GPCCHEM
Hello,
I apologize in advance for my poor English.
I used the GPCCHEM tool.
I attached the GPCCHEM data submitted and the report, could you please review it.
The report said
"Best chemical ID : 445 Best chemical ID max. deviation, % : 11.17
Summary of all IDs with max. DOD deviation below 15%
Chem ID max DOD error, % Max R deviation, ratio
445 11.17 0.48
461 12.01 0.4
6106 12.32 1.17
487 13.9 0.04
485 13.9 0.04
425 13.99 0.49
457 14.24 1.01
4124 14.34 0.53
Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge."
When I used the GPCCHEM tool before, the recommended value was less than 3% DOD deviation. (The chemistry was NCM then)
So I wonder whether 11.17% is really an acceptable value.
We would like to make SOC as accurate as possible. To this end, would you consider creating a new chemical ID?
Best regards.
Masami