Hello team,
My customer wants to use auto-retry mode at over current situation.
the datasheet mentions the delay pin connect pull up resistor to Battery line.
However, the datasheet mentions max voltage should be 7V.
Battery line should be 28V max.
Is this OK to pullup to battery line?
and what is the recommend value of resistance?
the datasheet doesn't have internal resistance value.
So, customer can not calculate pull up resistance value.
Best Regards,
Yuki