This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54260-Q1: Load Issue on TPS54260

Part Number: TPS54260-Q1
Other Parts Discussed in Thread: TPS54260

Specification 

Input Voltage : 9-60Vdc

Output Voltage : 5Vdc/2A

I made power supply with TPS54260. When i'm doing R&D testing without load it's working fine for full range(9-60Vdc). When i'm applying 500mA load @ input voltage 13Vdc output voltage dropped from 5Vdc to 0V gradually. Even after 13Vdc till 60Vdc it's happening the same. <13Vdc it's working fine. 

The issue i've noticed that SS/TR pin voltage is getting reduced from 2Vdc to 0.4Vdc after 13Vdc. 

I attached the schematic as well as waveform @ ss/tr pin on working condition(<13Vdc) and not working condition(>13Vdc).

   Working SS/TR pin 2Vdc  Not Working SS/TR pin 0.4Vdc  Working to Not  working when voltage incresed