We would like to keep ACDET High recongnization(ACFET/RBFET on) when the transition period to Hybrid boost mode around 100us as below.
Because heavy load is started, AC adapter's voltage will be down until start Hybrid mode, then it has possivility that ACDET voltage is lower than threshold.
(1) Can ACDET's ignore AC judge until go to Hybrid mode ?
(2) If ACDET port has the deglitch time by hard ware etc., please teach this time for just to make sure. (10ms/ 1ms / 1us / 1ns…)
(3). If ACDET port has not the deglitch time even though 1ns etc., when ACDET port level is High to low, if ACDET port level will be return to High immediatry, ACFET/RBFET will be not turn off? If is this correct,
please teach ACDET must be return High from Low within how many seconds for keep ACFET/RBFET still on?
Best regards,