Part Number: TPS22917
Other Parts Discussed in Thread: TPL5110, BQ25060, , LM66100, TPS25946
Hi,
I am designing a system that works with a Li-Po battery, has an on-board charger(BQ25060), and consumes nanoamperes(TPS22917L) when the system is in sleep mode(TPL5110). You can see the power block diagram of the system below.
When the USB is plugged in, the battery should be charged.
The system should be able to work from the USB port, sometimes with a battery and sometimes without a battery.

Everything works great here, except for the battery charging part, as you can imagine. And I realized this painfully after I produced the pcb and assembled the board.
The reverse current block in TPS22917 prevents charging.
Now what I want to ask here is, what kind of solution would it make sense to proceed with to charge the battery.
If I use a Load Switch without a reverse current block, how much voltage drop or current limitation will there be when the charge voltage passes over the diode of the mosfet inside?
Or would it be better if I put an ideal diode in parallel with the Load Switch(for example LM66100 or MAX40203 ) for battery charging, as in the block diagram below?

Other than these, I'd be happy to hear if you have any other solutions to suggest.
Thanks.