Other Parts Discussed in Thread: LM51551, LM51561
Hi , Does anyone have a problem with too high frequency when EMC ISN is testing, what can be solved?
LM51551, input 18V Boost to 48V.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi , Does anyone have a problem with too high frequency when EMC ISN is testing, what can be solved?
LM51551, input 18V Boost to 48V.

Hello Ted,
EMC is heavily dependent on the used external components as well as the layout of the board. A quick solution might be to use LM51561 with spread-spectrum instead. LM51561 is a pin to pin device and can be exchanged on the board for testing.
Best regards,
Brigitte