Hello TI Support,
I'm using a TPS55288 for outputting USB-PD power from 5 to 20 V and up to 3 A. The input is fixed at 14 V. This has been working well for the most part, but we are having issues when running at 5 V and very low load (a few mA). Under that condition, we have a large ripple on Vout, and since it's a 11 kHz, it creates an audible, high-pitch ringing sound.

I think that this is probably a result of instability in the loop compensation, but I'm not sure. The datasheet mostly talks about instability when operating in boost mode, but we're in buck mode going down from 14 V to 5 V. Are there best practices or recommended values for developing a compensation circuit that ranges from 5V to 20 V? Here is my current compensation values:

The other thing that seems to impact output voltage ripple is output capacitance and ESR. The Design Tool Excel sheet for TPS55288 recommends 81.3 µF of output capacitance for 50 mV of output ripple. We increased that to 123 µF on our design but are still seeing this issue. We have tried using just ceramic capacitors as well as using a mix of ceramic and low ESR ( 3 mΩ) electrolytic capacitors on the output.
Here is our full schematic:

Any help is appreciated.
Best regards,
Cory