Hi
When charging the battery with PMID instead of BAT, can it indicates the STAT pin?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
When charging the battery with PMID instead of BAT, can it indicates the STAT pin?
Thanks
Hi David,
If you have no battery connected at BAT pin you can expect the STAT pin to go back and forth between indicating charge in progress and charge complete due to the device automatically attempting to charge the BAT pin cap as if it was a battery. There is no way to adjust the functionality of STAT pin via I2C registers.
Best Regards,
Garrett
Hi Garrett
I have add a question.
Can I control the current if I use OTG function to output power to PMID?
Thanks