In bqeasy version 1.80, Sanyo's UR18650FM is assigned chemical ID 0100, which is a kind of default for 18650 cells.
In bqEasy V1.87, UR18650FM is assigned chemical ID 0135. I wouldn't question this development, except I am having trouble training my bq20z95. The capacity is spiraling into the weeds, going higher rather than lower, right now about 2x what it is supposed to be.
I have loaded another chemical ID, 0107, which is assigned to a similar 18650. So far, we are doing well.
Meanwhile, I noticed that the Chemical ID 0135 is also assigned to a very different cell, the UF103450. You may see a description here:
http://www.alibaba.com/product-gs/250752866/Li_ion_103450_battery_cell_Sanyo.html
This
battery is physically different than the one we are using, and the
capacity is much different (1800 vs 2500). I cannot explain why TI
would point us to a chemistry file for such a strange cell.
Is there even a *slight* possibility that the assignment of the UR18650FM to chem ID 0135 was in error?
Gratefully,
Michael A. Banak