Other Parts Discussed in Thread: TPSM82864A, TPSM82810
Hello,
I am designing a board whose delivery times to the customer are short. Therefore I am trying to find a DC2DC in stock that can work with the XILINX ZU7EV. There are currently no configured PMICs available. I wanted to verify whether the LMZ30604 component can be used to supply voltages to the ZU7EV component in a reliable way? the LMZ30604 can be configured to generate the required voltages, but I wanted to know if it is recommended or if something else that is available in stock is better.
The voltages are 0.85V, 0.9V, 1.2V, 1.8V.
Thanks!
Yossy Goldenberg