Hello,
is dimming with the SS/TR pin supported in PSPICE for the TPS62130? If so is there any guidance on how to implement this? we're having some issues getting that working.
thanks!
Nate
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Nate,
I just tested this out on PSPICE for TI and I was able to vary the Diode current based on the SS/TR resistor.
The datasheet gives the following guide on using this device for LED dimming.

Using a 0.1Ω resistor for R2 and a 50k resistor for R_ss/tr, I was able to produce 800mA current through the diode. When you vary the values of R_ss/tr it varies the LED current.
The expected current can be calculated from I_led = Vfb/R2. Where Vfb is given in the above figure.
Let me know if you are still having issues.
Thanks,
Joseph