This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24072: BQ24072 worked for a while but stopped charging

Part Number: BQ24072

Hello Dear,

It's the first I use BQ24072. 

It worked perfectly for a few times, and then It stopped charging the battery. The /CHG led blinks when I plugg my DC jack of 5V and it goes OFF. The Output is still working whether with Battery or with 5V DC jack.

So I don't think that the module is dead. I also tried to test the reverse polarity protection by putting the Battery in reverse, I don't know if it's that what caused the issue.

Can you help me please.

see below the schematic I used :

Thank you :)