Dear team,
For the current limit, my customer request the limit value should be larger than 5A in their application. Then Rlim=25kohm is not applicable because the minimum limit is 4.6A which is smaller than 5A. They need to set minimum limit is 5A, right? If so, how to calculator the minimum limit and maximum limit? Based on Rlim formula, we can only get the typical limit. For example, Rlim=20kohm, the typical limit is 7A, what is the minimum limit and maximum limit?
Thanks & Best Regards,
Sherry