Hello,
We are encountering an issue with the short circuit protection design from the slva998a.pdf application. We have implemented Figure 4.4 in the application. We have also adjusted the issue that the reference design had.
(please refer to this previous Forum Post: https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1086812/lmr62014-overcurrent-short-circuit-protection-for-boost-converter?tisearch=e2e-sitesearch&keymatch=slva998a.pdf#)
Below is the circuit we are using. The Rsense we have selected is 1ohm. This is just an initial value to confirm if the circuit is working. From computation we are expecting around 0.67A threshold current.
Here are the issues we are seeing, we are connecting a power supply in the input at 12V 1A limit.
The load that will be eventually connected to the output is a 12V FAN with the current draw of 300-350mA.
The initial setup we did to test the circuit was to test it with an electronic load set to CC mode at 350mA current.
The setup only works in a particular order of events in testing.
1. Connect Power Supply Cables to Input of circuit protection
2. Connect Electronic Load cables to Output of circuit
3. Turn ON power supply. Electronic Load CC mode is still OFF but the meter is reading the correct voltage.
4. Turn ON Electronic Load and the load is drawing the set 350mA current.
We also increased the current draw until we see the threshold. When electronic load CC mode current goes to 670mA, the output becomes 0V. Then it only goes back to 12V when we turn OFF the Load. The only issue is that it does NOT work if the electronic load is already ON. before turning ON the power supply.
We also connected an actual Load (FAN and resistors). The resistors were chosen so that it would draw similar current.
For both scenarios the FAN does not turn ON and the resistors do not draw the correct current when you connect it to the protection circuit then turn ON the 12V. The voltage measured in the FAN side is around 2V. The FAN also does not turn ON even if you connect the and turn ON the 12V first.
We then tried connecting a lighted load to the protection circuit (330ohms)
We tried both methods: connect load first then turn ON 12V and turn ON 12V then connect the load.
Connecting the supply first then load shows the correct current draw from the supply and voltage across the 330ohm resistor.
Connecting the load first then turning ON the supply shows 6V across the 330ohm resistor.
What might be the cause of these issues? Are there specific values that I need to use for the other components. Are there limitations with the having a lower current protection threshold not indicated in the application note. Does the values/type of load we connect to the current protection circuit affect its behavior?
Thanks,
Deniel