Hi,
I am using TPS53355DQPR in my design for below requirements:
1. Vin=12V, Vout=5V, Iout=30A
2. Vin=5V, Vout=0.84V, Iout=30A
Equation 8 in the datasheet provides a formula to calculate the inductor value. The equation contains Vin (max) value to be used during calculations.
Now what should be the Vin(max) value. Whether it should be maximum input voltage to the regulator as per my design which is 12V or maximum input voltage that the regulator can support i.e.15V. Please suggest.
Thanks!