Part Number: TPS60123
Other Parts Discussed in Thread: BQ25173, TPS61023
Hi everyone.
I'm building Power Multiplexing Using Load Switches using Boost converter.
My purpose: That's will switch Power supply between 5V_ISO(5VDC) and VOUT_BQ25173(4VDC) if any one of both power supply have problem.
Because VEN_H (Pin 2 of TPS61203) = 1.2V, so if my Battery lower 1.2V the output will OFF. I want to use maximize power off battery to supply to the Load when main power is loss, so I connected the Output of TPS61023 to EN pin through diode (Vf =200mA), it will run until battery < 0.5V.
Can you check my schematic and give me some advices for:
- This design for TPS61023 is correct, and it can run normally?
- Do you have another solution for my idea?
- If my design is correct, can you give me some diode have lowest Vf?
Thanks for your support