Hello,
I'm using a TVL73333PDQNR device.
I would like to ask you about the inrush current at startup.
The circuit diagram is shown below.
The current is measured at the red circle at startup, but 512mA flows at the peak.
It is considered that such a peak current is generated due to the charge to the output capacitor.
In steady state, it is 49mA.
(Question 1)
Is it okay to go into a foldback current limit every time the device boots?
Please let me know if you have any concerns.
(Question 2)
Does the foldback current limiting function take into account the inrush current due to charging the capacitor?
Or is it considered only in the case of a short circuit?
Best regards,