This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62067-Q1: PWM/PFM transition ISSUE

Part Number: TPS62067-Q1
Other Parts Discussed in Thread: TLV62065, TPS62067

Hi,

The customer used TPS62067-Q1 to power the video decoder in the instrument cluster.

The schematic has not been modified.

TLV62065 (before) to TPS62067 (after)

As a result of the review as an issue that appears to be video noise in VIDEO DECODER, it seems that it is automatically changed to PFM mode.

Load current : 450mA

Load conditions require PWM mode operation.

However, the waveform appears to be entering PFM mode.

Refer to the graph, I have to do the PWM operation, but I don't know why it looks like PFM.

Q1. Is the blue area PFM correct? Or what kind of mode is it?

Q2. Please advise if there is any way to improve intermittent PFM.

  • Hi Cho,

    Thanks for your question.

    The blue area seems indeed like PFM, since the SW node voltage is not bounded to either VIN or GND.

    In order to confirm, could you please also check the inductor current (together with SW node)?

    That would give us a better understanding of what is really happening.

    Thanks,

    Stefano