Hi team,
what’s learn mode and peak shift mode?
![]()
would you help elaborate?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Fred,
LEARN function allows the battery to discharge while the adapter is present. It
calibrates the battery gas gauge over a complete discharge/charge cycle.
When the battery voltage is below battery depletion threshold, the system
switches back to adapter input by the host. When CELL_BATPRESZ pin is
LOW, the device exits LEARN mode and this bit is set back to 0.
Khalid