This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25982: Potential Cause of Chip Damage

Part Number: TPS25982


Hello,

We have used eFuse chip TPS259827ONRGER in our product. Recently, we have a malfunctioning board returned from our customer. We found two of the eFuse chips were physically damaged. It seems that one is totally burned and the other also has a bulge on its top surface, as shown in the pictures below.

      

We have tried to figure out the root cause of this kind of damage.

First, we suspect if it is really caused by extremely high current going through it. But it seems there is no indication on the output side of eFuse on the board, there is no burned PCB traces or connector pins. And eFuse chip is supposed to shut down its output when high current appears. So we think it is unlikely because of the high current.

Then, We are thinking if any reverse voltage can cause the damage. We have reverse protection at eFuse input, but not output. Then we tested to connect +5V, +12V, +24V, -5V, -12V and -24V at the eFuse output without supply power on its input side. and above test didn't damage the eFuse. Of course, when all negative voltages were applied, they were clamped to -1V by a TVS (SMAJ24A-13-F) at the output of our board.

Last, we wonder if any shortage on eFuse output side (there is more damage on that burned chip on its output side) could burn it. For example, some shortage between the board and metal enclosure for whatever reason. But we have tested that output shortage is also protected by eFuse and this is also a function and feature of the eFuse chip.

The schematics of the eFuse is shown below. Do you have any suggestions of the cause of this kind of damage. Is there other users experiencing similar thing? Thank you!

Best Regards!

Michael

  • Hi  Michael,

    Thanks for reaching out. Please help with below info:

    1. How many boards failed and how may were tested?

    2. Did it fail on first power up?

    3. After what test it failed?

    4. What is the result of ABA swap?

    5. What is the input voltage? and was load drawing some current when fail happened?

    Regards

    Kunal Goel

  • Hi Kunal,

    1. Up to now, this is the only board failed and returned by our customer. We have tested all the boards (a few hundred) before shipping out.

    2. I am quite sure it didn't fail on the first power up. However, there is very limited feedback information from our customer either. They told us that our product and all the load (LED strips) worked well together at first. After two of the LED strips failed, they replaced them but the new ones still didn't work. So they sent back our product. After removing the enclosure, we found two of the eFuse chips were damaged.

    3. As mentioned above, it seems the eFuse failed during LED application on customer's site, but we don't know any more details from the customer.

    4.We didn't do the A-B-A swap, because some pads on the PCB beneath that burned eFuse chip are also damaged. The customer also bought several same products to for their LED strips, the problem only happened on this board.

    5. The input voltage can be 5V DC, 12V DC, or 24V DC. In customer's application, they use 24V DC. Since the LED strips were discovered not working, I assume there was some current draw when eFuse failed, not quite sure how much current and how it burned the eFuse while the connector pins seems intact.

    Best Regards!

    Michael

  • Hi Michael,

    Thanks for the info.

    I am thinking transients exceeding device abs max rating of VIN and VOUT pin could be the reason. First thing is VIN is 24 so chances of violating VIN abs max spec is high. Also if LED strip failed in short then device must have turned of quickly to limit the current and that can give rise to negative transient on VOUT pin which can exceed abs min rating of VOUT pin.

    So it is recommended to use TVS at input and schottky diode at output pin close to the pins.

    Please refer datasheet section 10.1 Transient Protection for more details.

    Regards

    Kunal Goel

  • Hi Kunal,

    Thanks for your suggestion.

    We will have more investigation to seek a solution to prevent overvoltage and damage to the eFuse chip.

    Thank you!

    Michael