Other Parts Discussed in Thread: BQ51003, BQ51020, BQ25170, BQ51221, TIDA-00243
Hello,
I read the user manual about dimensioning RFOD and understand, that this has to be checked on the final product with a calibrated transmitter and the necessary tools.
But with what default value should I start?
I downloaded the "FOD Calibration" Tool to find out the default value, but the BQ51222 is not listed there.
I choosed BQ51222 because of the low price (compared to the others) and the high stock of this product.
I read many threads about the BQ51222 because it seems like TI is not recommending it if only one standard is used.
<<<
" .. The BQ51222 makes a number of compromises to meet WPC and PMA. "
>>>
What are those compromises?
I plan to wireless charge a small battery (140mAh), with a receiver current of max 280mA (140mA for the product and 140mA max. for charging).
BR, Alexander Sevcik