This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54116-Q1: Please explain the waveform at startup.

Part Number: TPS54116-Q1

hello.

I made a board design with TPS54116-Q1.

The design is 1.35V output, and the startup waveform is as shown below.

In the simulation of WEBENCH® Designer, when the load is 0.1A, it looks like the figure below.

In the simulation of WEBENCH® Designer, when the load is 1A, it looks like the figure below.

In my design, it is almost not loaded at startup.

I would like to know why the voltage waveform is not a ramp waveform but drops once at startup.

Also, can you guess the reason why it is 0.2V in the simulation but 0.6V in the actual measurement?

Thanks,