This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD17559Q5: MOSFET replacement

Part Number: CSD17559Q5
Other Parts Discussed in Thread: CSD17575Q3

Please recommend a MOSFET that can replace ON-FDMC8010, the Rds(on) is required to be less than 1.2mR,
and requires the same package
  • Hello Shawn,

    Thanks for the inquiry. The FDMC8010 is 30V, 1.3mΩ N-channel FET in 3.3x3.3mm PQFN. Our closest cross is the CSD17575Q3, 30V NFET in 3.3x3.3mm SON but the resistance is higher, 2.3mΩ max at VGS = 10V. We don't have any FETs with lower resistance in the same package. The CSD17559Q5 is in the larger 5x6mm SON package and is not a direct cross.

    Best Regards,

    John Wallace

    TI FET Applications