Other Parts Discussed in Thread: BQSTUDIO, EV2400
Hello,
We are using BQ27411-G1C for one of our projects.(We are using a battery with 3200 capacity, 3.7 volt nominal voltage, cut off current of 50 mA) I have questions about a few parameters:
1 - In the IT cfg register I use typical values for all parameters except, user Rate-PWR. I dont understand how to calculate the correct value. I would appreciate if you can help me with this parameter.
2 - For the taper current i choose cut off current(50 mA) as the limit. Is this a right assumption?
3 - For the "Ra Table Class", do i have to do any operation, or the gauge calculates these values itself? Since this is an handheld device, it is possible that battery would go to 0 V and gauge would lose its calibrations(If there is any). Would this effect, correct SOC calculation when battery starts charging until calibration is recalculated? If so, is there any way to avoid re-calibration everytime gauge is powered-on. (Please note that ROM is not programmed in my device, therefore i have to load register settings manually if power on reset is detected)
4 - Battery management studio says it does not support BQ27411-G1C. Therefore, i dont know how to program ROM of the device. Is there any way to do it without golden image?
Thank you,