Other Parts Discussed in Thread: USB2ANY
Hello,
I got 2 dev.kit, BQ79656EVM and BQ79616EVM. I don't have USB2ANY device.My problem is that just at the first try, it seems in both kits, the BMS is not awake after I connect the supply.
I did these:
- to use internal resistor ladder: short all S1 and S2, short J14 and J16. Later, I can see voltage steps on Cell-x (white test points near to J15 connector) as expected.
- connect external power supply (i tested both 33V and 50V) to PWR and GND.
using test points, I observe:
- BAT pin is same as PWR, then BMS gets the power.
- NPNB (of Q1) is 5.0V, but I expected > 6.5V.
- Then the LDOIN is also 4.5V, but I expected 6.0V, as written in datasheet.
- Both CVDD and NFAULT pins are also 4.5V.
I have also some samples from both BMS chips. Then if it seems the chip is damaged, I can replace them.
Best regards.