Hello,
We try to use the LM3410XSD as backlight driver with an output of 16V@360mA. Our Prototype is working fine but we have some EMI issues in the range of 240-290 MHz. Even if we pass the quasi-peak measurement in this range we are a little bit afraid that it was just luck for this time.
Here are the results of the EMC laboratory

Picture 1: Antenna - Horizontal

Picture 2: Antenna - Vertical

Picture 3: Quasi-Peak Table
We think that the source is the backlight converter because of some remeasurements using a spectrum analyzer and a near field probe.
Picture 4: Remeasurement - Measurement Point

Picture 5: Remeasurement - Results - Backlight on

Picture 6: Remeasurement - Results - Backlight off
Here is a picture of our schematic.

Picture 7: Schematic of backlight convertion
Do you have any hints how we could improve the results?
Best regards
Janis