Other Parts Discussed in Thread: TLV62595, TPS2597
Dear Team,
Hope you are doing well.
I got a question from the customer during the use of TPS25923.
The typical overvoltage clamp of TPS25923 is 6.1V and can reach to the max value of 6.75V. The datasheet is shown as figure below.

The buck converter the customer used is TLV62595, which has the maximum input voltage value at 6V. The datasheet is shown as figure below.

Could the buck converter be protected by the efuse TPS25923?
Does This efuse protect the circuit through both current and voltage?
I'm looking forward to your reply.
Really appreciate your help!
Best regards,
Xenon Li