Other Parts Discussed in Thread: TPS3851
Hi Team,
Is it acceptable and safe to drive the WDI pin of UCC3946 to 3.3V when VDD is not supplied to the device (UCC3946 is powered-off)? The datasheet does not specify a VIH maximum for this pin - so our customer want to double-confirm that driving WDI to a voltage higher than VDD would be fine.
They do not intend to exceed the specified the 10V absolute maximum rating. Thanks in advance!
Kind Regards,
Jejomar