Other Parts Discussed in Thread: TPS548A28, , TPS548A29, TPS548B28, TPS53318
Hi support team.
My customer asked me regarding behavior when VDD is 4.5V.
Recommended operating condition of VDD is 4.5V to 25V
In addition, Minimum VREG Spec in datasheet is 4.77V at VDD = 12V.
I think that minimum VREG output voltage will be 4.25V when VDD is 4.5V.
In this case, my customer is concerned about the behavior of internal circuit.
(Especially, there is no abnormality in the protection circuit)
Does it work fine even if VDD is 4.5V?
Best regards,
Higa