This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5088: Pin 9 OUT

Part Number: LM5088

Hi Team, seeking some clarification. 

The LM5088 datasheet instructs the designer to connect Pin 9 (OUT) to the output Voltage (Vout). The abs. max. table does not specify a limit for pin 9 thus the default is 7 V. Is this correct? and thus the max output voltage for the LM5088 is 7 V?

Thank you.

-Mark