We are having a requirement to design 115VAC/400Hz to 24VDC 50W Power Supply.
can any one suggest me to which ic i can use this application
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
400 Hz is the line frequency generally air craft or ship power. So you just need a a bridge rectifier which that design has.
I marked up the schematic to show the AC to DC converter using a bridge rectifier and storage capacitance. Then you step down the DC voltage to 28V in a DC to DC flyback converter. I believe the control IC in this design is a UCC28610 and this reference design would work in your application for 50 W.
On your other post I had recommended using the UCC28711 or UCC28704 and recommended to reference designs as well for the 5 W application.
Regards,