This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24079: Could charge current change while power on

Part Number: BQ24079


Dear Specialists,

My customer is considering BQ24079 and has a question.

I would be grateful if you could advise.

---

Is there any problem in switching the logic of "EN2 terminal" and "EN1 terminal" while 5V is applied to the "IN" terminal of the bq24079?

・Normally, EN2 is set to 1 and EN1 to 0 (current value depending on external resistance: 1.09A according to the Li-ion battery specifications used).
・When a personal computer is connected, considering USB-2.0, set EN2 to 0 and EN1 to 1 (USB500mode), 0.5A.

---

I appreciate your great help and cooperation.

Best regards,

Shinichi