Other Parts Discussed in Thread: LM5146, CSD17308Q3, CSD18532Q5B, CSD18534Q5A
Hi every expert, my design is as below.
LM5141QRGERQ1 design:
switch power supply: input 24V
battery supply:14V-16.8V
output voltage12V,output current need 10A,
power inductor: Air core inductor 3.3uH
Fsw=2.2MHz
DEMB-VCC,FPWM mode
I want to know if my design is ok to have output 12V/10A with above design.
Now I can get output 12V/3.5A when R19B is 12mΩ,while when R19B is 0Ω the output current can reach 5A.
My question is if I want to get stable 12V/10A, what can I do?
I am glad to get a good answer.Thank you.