Is there any reason not to put two PTH08080W on the same pcb sharing the same input voltage (but not the output) ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any reason not to put two PTH08080W on the same pcb sharing the same input voltage (but not the output) ?
The PTH08080W must not share the inhibit pin or Vout Bus .
Each PTH08080W , inhibit pin , must have their separate open drain control FET. The inhibit pin must not be pulled up externally to Vin or any other voltage. The PTH08080W has its own internal pull-up to about 1.5V.
The PTH08080W is not parallelable for increased output current . This operation will overstress the module.
Tom