I was using PSpice for TI to run the simulation for this project, but I got this error where I have too many imported components. So I decided to edit the schematic on Altium instead.
After I started simulating on Altium by importing the file from OrCAD. I found out that my voltage source (on the left) is not giving any voltage, so I changed it to the VSRC (on the right), and was able to output correctly voltage in the operation point. (I added the Pspice simulation model to each of the imported components)
However, after that, I wasn't able to simulate the schematic anymore because it kept showing the error "Transient Analysis: Time Step Too Small". But my transient simulation parameter did not change.
So I started changing the parameter around. Changed the stop and step bigger (or smaller), and still not working.
I also changed the "affect" file from document to project in the simulation dashboard, and it also doesn't work.
I tried to simulate a regular circuit, a buck converter using the VSRC as my input voltage and PWM signal (VSRC can change to pulse wave) to see if I would get the same error. But I was able to simulate the schematic successfully with the correct simulation graph.
So I am not sure how to fix the error.
Here is my schematic for my project.
(I modified this schematic with the VSRC source, and was unable to simulate it due to the error)
(Have not yet modified the voltage source yet, but was able to simulate the transient graph without the error.)