Other Parts Discussed in Thread: BQ24079T
Hello.
I am testing the overcurrent protection operation of the TPS25947.
A BQ24079T is connected downstream of the TPS25947 to charge a 1-cell lithium-ion battery.
The downstream of the TPS25947 and the lithium ion battery are configured with a diode OR connection to supply power to the system.
The overcurrent protection is designed with a setting of 2.5A.
When an electronic load (CR mode) is connected downstream of the diode OR and a load is applied, intermittent operation was observed as shown in the attachment.
With the lithium-ion battery unconnected, there is no such operation, and the device turns off when the overcurrent threshold is exceeded.
Do you know the cause of this problem?
Thank you in advance.