Hi Team,
How can I adjust the slew rate of the load current when I use PMICLOADBOARDEVM?
Best Regards,
Tom
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
How can I adjust the slew rate of the load current when I use PMICLOADBOARDEVM?
Best Regards,
Tom
Hi Tom,
The PMICLOADBOARDEVM is like voltage controlled current sink. Meaning that that you control the output current by input voltage level and therefore also slew-rate is controlled same way.
So in practice when you drive 0 - 100 mV voltage signal in 1 µs to input you will get 0 - 2 A load transient in 1 µs on output.
BR, Jari