Hi,
My configuration is 2S LiFePO4 where my battery can discharge from 7.2v to 5V or say 5.2V.
So as per understanding from the datasheet(section 11), my battery depletion threshold should be 5.2V
With adapter absent my battery is connected to VBAT and load is connected to VSYS.
As per the datasheet (section 11) and above explanation, should my VSYS_MIN be 5V?
And if I let VSYS_MIN be 6.6V (which is default for 2S) , should discharge through VSYS be discontinued once overall voltage drops below 6.6V?