Part Number: TPS65988EVM
Hi Team,
A customer is designing a two-port USB C PD3.0 product by using the chip TPS65988DHRSHR, the application is a pure PD. They also decided to use TPS65988EVM module design as a reference.
The customer is requesting assistance for their design:
1. USB port#1 has to support all the profiles starts 5V/3A(15W) - 20V/5A (100W)
2. USB port#2 has to support upto 25-30W power delivery but should support all the voltage levels from 5V-20V , for example: USB port#2 shall support 5V/3A, 9V/3.3A,15V/2A,20V/1.5A, is it possible to configure the same?
3. They are planning to use the LM3489QMM/NOPB for both the ports. Kindly advise.
Thanks in advance.
Regards,
Marvin