I am looking at the BQ25181 to act as a battery charger and system voltage regulator in my wearable device. The device will be powered from a 3.7V li-po battery - will the BQ25181 still be able to provide a 4.5V regulated output on the SYS pin both when a power supply (USB) is present and when running off battery? If not, is there a single device that can do this, or will I need a charger IC and a boost converter (eg. TPS61099x)?