Part Number: TPS62865
Other Parts Discussed in Thread: TPS62827
Hi Team,
My customer need a buck converter solution which efficiency performance can meet below requirement. I found performance of TPS62865 close to customer's spec. Do we have better solution?
1. VIN: TBD. 3.3V, 5Vor 19.5V are okay to use.
2. Vout: 0.75V
3. Iout: Maximum 1.5A.
4. 88% efficiency at 10mA load
5. 88% efficiency at 100mA load
6. 91% efficiency at 1.5A load
Best regards,
Hardy