Hi,
Setup : Input 8V to 18V
Output : 20V - 35V, 700mA (as in the EVM)
While using the evaluation board ,when the Input voltage remains constant at around 4.2V then MOSFET Q2(Si7854DG ) gives a beeping sound and after around 5 seconds it blows up. This situation is when the voltage cut off is set at 4.5V.
Next when we have increased the input voltage cutoff to 10V, then at around constant input voltage of 9.3V the MOSFET again gives a beeping sound and blows up.
What is the reason for this failure??