Hi team,
Could you please let me know how to make sure VDD5 is powered by external supply?
The datasheet 7.3.2 mentions the external supply should be higher voltage than the LDO regulation voltage programmed by (B5h) USER_DATA_05 (POWER_STAGE_CONFIG).

In default, the maximum LDO regulation voltage looks like 4.9V.
Looking at Figure 7-4, I wonder how we can know that VDD5 is working with external supply because the forward voltage of the diode should be considered.

If the maximum forward voltage of the diode is 0.35V, should the anode voltage (i.e. external power supply voltage setting) be calculated as below?
Vin_max+ Vf_max = 4.9+0.35 = 5.25[V]
I wonder why 4.75V-5.25V anode voltage is enough to operate external VDD5 considering the forward voltage drop.
I think this is important for efficient power design.
Best regards,
Itoh