Other Parts Discussed in Thread: LM5155
Hi Ti Team,
Through aid of Ti Webench I could design Boost Converter for below specifications
Input Voltage: 10V to max 17V
Output Voltage: 24V, 3A
Switching frequency - 460KHz
With Resistor divider circuit at FB pin 51k and 2.2k and board works fine (Pls refer report attached and sch image)
Now I would be like to change it to 510k and 22k respectively to reduce current consumption.
As there is no option to simulation and verify webench could you help on this regard ?
Will it be any concern if change of resistor ?