hi
I'm looking for external circuit to over current limit
In my case , I use auxiliary power supply that output voltage is 12V , no bias VCC
- using Isolate CT, R35 connects CS and GND
even UCC2801 have over current limit circuit that CS voltage over 1.5V
the converter that using UCC2801 maintain constant current - Load set short current therefore output voltage is zero
UCC2801 is current mode controller so that situation can be appear
but other device will destroy because short circuit continue during long time
so the converter need external circuit that output current (or CS voltage) is over limit point, that operate hiccup mode
I think using internal comparator is best option, how can i do?