This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51013B: comparing bq51013B and bq51003

Part Number: BQ51013B
Other Parts Discussed in Thread: BQ51003,

Hi everyone

we are looking to add wireless power to a client product.

we select the bq51003 because of its low price (0.48$ @1000) but because it is out of stock we choose bq51013B which is a pin-to-pin compatible with bq51003, the only difference that we can see from the datasheet is it the output power (bq51003 is optimized for 2.5W)

we are hoping that we can use the bq51003 when it is in stock. 

and we wanna know if the only difference is the power optimization and if that can be a problem if we change the two IC in the future.

thank you.