This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL2845: Does the TL2845 support frequency dithering?

Part Number: TL2845
Other Parts Discussed in Thread: UCC28180, TLV3201

Hi,

I'm using the TL2845 current mode PWM controller for a DC-DC converter operating at a certain constant frequency. I'm aiming to add a frequency dither so that I can reduce the EMI peaks. My requirement is very similar to how frequency is dithered on the UCC28180 on the SLUA704 document. However, the UCC28180 has a simple resistance where we supply an additional dither current to change the frequency. On the TL2845, it is not simple as there is an Rt-Ct combination that decides the switching frequency. Are there any design examples or procedures to follow to obtain dither on the TL2845? Is a frequency dither even possible on the TL2845?

Thanks

Santhosh