We are using BQ24617 battery charger in our project. can you help us on the following issues.
1. We have connected the thermal shutdown pin of the battery to the TS pin of the charger. At certain temperature (example 45˚ C)
a. How will the charger suspends the charging of the battery
b. Does it indicate through the status signals to shut down the system.
2. When the DC adaptor is not connected and only battery connected, how can we shut down the system below certain voltage level.
3. When the DC adaptor is removed, How can we use the STAT 1, STAT 2, PG signals to identify the DC adaptor present.
4. One more issue we are facing in the battery controller is in reading the charge units. The VFB pin is connected to an ADC and it’s output is read through SPI of the Microcontroller. The value read from the SPI is 0 or greater than 3000 sometimes. The reasonable working ADC values range between 1500(low charge condition) and 2100(full charge condition) approximately. Also we would like to know the cut off voltage at which the software should put the system off for the battery to come longer.
Regards/
Vengat