Other Parts Discussed in Thread: BQSTUDIO, GPCCEDV, BQ40Z50
Hi,
I have a BQ4050 in my design and we've seen numerous issues where the SoC is very wrong. Specifically, when we are near the top or bottom of the battery voltage range it will have some SoC number more in the middle (38% when near full, 0% when battery voltage is only at 3.4V per cell). In our normal use case we don't charge the battery to full or discharge to empty so it is designed to be discharged/charged from 30-80%. That being said I have taken the pack down to 0 and up to full several times to see if it corrects this issue but it does not.
What is going on here? Is there a error in or parameters or the way we're using the gauge? Our cells are typical 18650 so nothing to special there.
Thanks,